masserase memory map

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

masserase memory map

1,575 Views
Neo_zhang
Contributor II

CW execute masserase, which part the memory has been erased?  both EEPROM and flash or just the flash ?

0 Kudos
Reply
2 Replies

1,558 Views
stanish
NXP Employee
NXP Employee

Hi,

Could you please specify the target MCU you are using?

In case it is S12(x) family there is an option to enable/disable erasing of EEPROM (go to File -> Configuration dialog - where you can specify which flash memory blocks should be erased:

stanish_0-1709902761322.png

If you use S12z the debug will erase just Program FLASH. in order to program EEPROM you should use Flash Programmer component (Target Task): 

stanish_1-1709903067485.png

 

Hope it helps.

Stan

 

0 Kudos
Reply

1,555 Views
Neo_zhang
Contributor II

My target MCU  is MC9S12DT256, can I edit 0x000 - 0x3FF registers region and 0x1000 - 0x3FFF RAM and how to do it?

0 Kudos
Reply