co-relation between instruction and clock/bus cycle

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

co-relation between instruction and clock/bus cycle

2,791件の閲覧回数
applejuice5
Contributor I

for S12 family there is mentioned core clock and bus clock, which is half the core clock.

now each instruction cycle is one bus clock or core clock ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,158件の閲覧回数
jsmcortina
Contributor III

If you haven't already seen it, then take a look at the S12XCPU datasheet. That lists each instruction and its cycle count.

 

Looks like S12XCPUV1.pdf is still the current version.

 

James

0 件の賞賛
返信

2,158件の閲覧回数
MJW
NXP Employee
NXP Employee

Hello,

 

the correct version of the CPU reference manual depends on the actual MCU family used:

 

* most S12 devices generally refer to the S12CPUV2 Reference Manual (S12CPUV2.pdf, latest Rev as of today: 4.0)

 

* some S12X (e.g. S12XD) refer to the S12XCPUV1 Reference Manual (S12XCPUV1.pdf, latest Rev as of today: 1.01)

 

* most S12X (e.g. S12XS, S12XF, S12XE) and recent S12 devices (e.g. S12P) refer to the CPU12/CPU12X Reference Manual (S12XCPUV2.pdf, latest Rev as of today:1.03)

 

This last document mentioned above actually describes the all existing ISA versions for CPU12 and CPU12X.

 

HTH,

MJW

 

0 件の賞賛
返信

2,158件の閲覧回数
kef
Specialist I

Shortest instruction (like NOP) take one bus cycle.

0 件の賞賛
返信