boot loader-MM912G634DV1AE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

boot loader-MM912G634DV1AE

1,949件の閲覧回数
adelantesey
Contributor IV

Hi

I want to start run boot loader of MM912G634DV1AE , everybody have any experience for this Mirco? we want use LIN , is there any sample code?

Thanks.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,651件の閲覧回数
iggi
NXP Employee
NXP Employee

Unfortunately there isn't LIN bootloader developed for this device.

We have example codes which demonstrates LIN communication written for other device based on similar core as on MM912G634. That could be of help. You could re-use the code, since the registers are quite the same.

With that, writing your own bootloader could be a nice challenge and here are some things about that to consider:
Re: CAN bootloader for mc9s12xep100

Regards,

ig

1,651件の閲覧回数
adelantesey
Contributor IV

Dear Iggi

Thanks for your replay, you mean is there is no LIN bootloader in this time or is it impossible that we we will implementation LIN bootloader on the this device?

0 件の賞賛
返信

1,651件の閲覧回数
iggi
NXP Employee
NXP Employee

Hello,

i mean 'there is no LIN bootloader in this time'.

LIN bootloader can be implemented on any device with LIN module.

Regards,

iggi

0 件の賞賛
返信