boot loader-MM912G634DV1AE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot loader-MM912G634DV1AE

1,930 Views
adelantesey
Contributor IV

Hi

I want to start run boot loader of MM912G634DV1AE , everybody have any experience for this Mirco? we want use LIN , is there any sample code?

Thanks.

Labels (1)
0 Kudos
Reply
3 Replies

1,632 Views
iggi
NXP Employee
NXP Employee

Unfortunately there isn't LIN bootloader developed for this device.

We have example codes which demonstrates LIN communication written for other device based on similar core as on MM912G634. That could be of help. You could re-use the code, since the registers are quite the same.

With that, writing your own bootloader could be a nice challenge and here are some things about that to consider:
Re: CAN bootloader for mc9s12xep100

Regards,

ig

1,632 Views
adelantesey
Contributor IV

Dear Iggi

Thanks for your replay, you mean is there is no LIN bootloader in this time or is it impossible that we we will implementation LIN bootloader on the this device?

0 Kudos
Reply

1,632 Views
iggi
NXP Employee
NXP Employee

Hello,

i mean 'there is no LIN bootloader in this time'.

LIN bootloader can be implemented on any device with LIN module.

Regards,

iggi

0 Kudos
Reply