Why is the current consumption so high?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why is the current consumption so high?

1,312 Views
xiaokangkp
Contributor III

When i make the MCU(MC9S12G128) go into full stop mode with the API interrupt enabled,why the current consumption so high: about 7.5 mA ?  The datasheet of G128 in page 1195 said API enabled(with interrupt is disable) just take 24 uA.

pastedImage_2.png

My codes is as follows:

pastedImage_4.png

pastedImage_5.png

pastedImage_3.png

is there something wrong? if i disable the function   // API_timer_start();  in  Enter_FSTP_Mode(), the current of all is only about 18 uA.

0 Kudos
Reply
1 Reply

1,163 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

What do you drive with PT0?

Please try the attached example.

Regards,

Daniel

0 Kudos
Reply