Using MC9S12DP56B with Flexray Daughter card MFR4300

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using MC9S12DP56B with Flexray Daughter card MFR4300

2,304 Views
brian_s
Contributor I
I am uundertaking a project for college to set up a flexray network. I have a HCS12 development board which I was hoping to attach a flexray daughter card to. From the information I am findidng on the site, the MFR4300 seems to be my best option. Am I correct in thinking I also need an adapter board to attach the daughter card to the development board (M68KIT912DP256)? Where would I be able to purchase this adapter card?

Thanks
Brian
Labels (1)
0 Kudos
Reply
1 Reply

1,274 Views
vikram_iyengar
Contributor I
search for SCFLXRAYADPTS12. It supports MFR4200 and 4300. Good luck with the project.
0 Kudos
Reply