Updating a MC9S12DP256 design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Updating a MC9S12DP256 design

3,140件の閲覧回数
Trace
Contributor I
Hi,
I'm currently updating a design and I can see that the processor used is gone obsolete. Which processor should I use instead? I'm using the external bus in my design.

Best regards
Jan Thogersen
ラベル(1)
0 件の賞賛
返信
1 返信

1,214件の閲覧回数
EMontanez
NXP Employee
NXP Employee
Jan,

What is the complete partnumber and maskset you are using? I don't see the DP256 going away anytime soon...I do know however that many parts are changing partnumbers to be RoHS compliant. Also, the DP256 went from a "DP256B" to a "DT256" and updated some flash reliability.
0 件の賞賛
返信