The ADC of the MM912F634

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The ADC of the MM912F634

跳至解决方案
821 次查看
guofeng
Contributor II

Hello!

I have read the datasheet of the MM912F634, but I did not find the section to describe use the ADC.

if the PTB analog input use 2.5V as reference voltage. How about the VSENSE? The voltage of VSENSE can up to 27V. 

Is there have a method to calculate?

QQ截图20171010204309.png

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
629 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Guofeng,

As you can see in the MM912F634 datasheet, the ratio of the VSENSE input divider is 10.8, so at VSENSE = 27V, the measured voltage will be 27V/10.8 = 2.5V and ADR10 = 0xFFC0. At VSENSE = 13.5V, the measured voltage will be 1.25V and ADR10 = 0x7FC0.

Table 24.JPG

Hope it helps. If you have any other questions, please let me know.

Best regards,

Tomas

在原帖中查看解决方案

2 回复数
630 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Guofeng,

As you can see in the MM912F634 datasheet, the ratio of the VSENSE input divider is 10.8, so at VSENSE = 27V, the measured voltage will be 27V/10.8 = 2.5V and ADR10 = 0xFFC0. At VSENSE = 13.5V, the measured voltage will be 1.25V and ADR10 = 0x7FC0.

Table 24.JPG

Hope it helps. If you have any other questions, please let me know.

Best regards,

Tomas

629 次查看
guofeng
Contributor II

Hello Tomas,

Thank you for your answer.

I has found this from the Chapter 3 Electrical Characteristics. Thank you very much!

Best regards,

Guofeng

0 项奖励
回复