The ADC of the MM912F634

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The ADC of the MM912F634

Jump to solution
820 Views
guofeng
Contributor II

Hello!

I have read the datasheet of the MM912F634, but I did not find the section to describe use the ADC.

if the PTB analog input use 2.5V as reference voltage. How about the VSENSE? The voltage of VSENSE can up to 27V. 

Is there have a method to calculate?

QQ截图20171010204309.png

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
628 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Guofeng,

As you can see in the MM912F634 datasheet, the ratio of the VSENSE input divider is 10.8, so at VSENSE = 27V, the measured voltage will be 27V/10.8 = 2.5V and ADR10 = 0xFFC0. At VSENSE = 13.5V, the measured voltage will be 1.25V and ADR10 = 0x7FC0.

Table 24.JPG

Hope it helps. If you have any other questions, please let me know.

Best regards,

Tomas

View solution in original post

2 Replies
629 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Guofeng,

As you can see in the MM912F634 datasheet, the ratio of the VSENSE input divider is 10.8, so at VSENSE = 27V, the measured voltage will be 27V/10.8 = 2.5V and ADR10 = 0xFFC0. At VSENSE = 13.5V, the measured voltage will be 1.25V and ADR10 = 0x7FC0.

Table 24.JPG

Hope it helps. If you have any other questions, please let me know.

Best regards,

Tomas

628 Views
guofeng
Contributor II

Hello Tomas,

Thank you for your answer.

I has found this from the Chapter 3 Electrical Characteristics. Thank you very much!

Best regards,

Guofeng

0 Kudos
Reply