Simple question! - MC9S12XEP100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simple question! - MC9S12XEP100

1,546件の閲覧回数
kayji
Contributor I

I just would like to know how fast the system clock is in default setting. Since the crystal oscillator providing frequency to board is only 4MHZ, i just wonder whether real system clock is 4MHZ.

And if it is, anyone know how can use more than 4MHZ, may be 16MHZ clock speed?

ラベル(1)
0 件の賞賛
返信
1 返信

1,287件の閲覧回数
vishaka_maithil
Contributor I

hi dear,

 

If your board has a 4MHz crystal then the bus /clock speed will be 2MHz (for XEP100). If you want 16MHz  clock speed with the same 4MHz crystal , you may use PLL for your application.

0 件の賞賛
返信