Serial Communications not working correctly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Serial Communications not working correctly

1,704件の閲覧回数
rayhall
Contributor V

Hello,

 

I am new to Freescale products, and have been using Atmel AVR in the past. I have
the EVB9S12XEP100 and trying to lean how things are done. I used Processor Expert
to create the  code for the serial communications. The code below does send data, but
all I get is garbage. Baud rate for code and terminal software are the same.

This is all the code TestComms.zip

Ray.



const uint8_t okay[6] = {0x24,0x4F,0x6B,0x61,0x79,0x7E};   // "$Okay~"//------------------------ Delay ------------------------------static void delay(void) {  volatile unsigned long i;  for(i=0;i<50000;i++);}//---------------------- USART TxString -----------------------void USART_TxString(const uint8_t StringPtr[], uint16_t len){   while (len--) // send len bytes   {      if (AS1_SendChar(*StringPtr) == ERR_OK){                     StringPtr++;      }   }}//------------------------- Main ------------------------------------void main(void){   PE_low_level_init();    for(;;){       delay();      USART_TxString(okay, 6);         }
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,462件の閲覧回数
rayhall
Contributor V

Problem solved. Used the SendBlock function.

 

Thanks for all the help..:smileywink:

0 件の賞賛
返信

1,462件の閲覧回数
rayhall
Contributor V

Okay I have found the cause. Jumpers J111 and J112 were not set correctly, and the wrong clock source was selected.

I still have a problem. I am not receiving the full number of bytes.  Only getting the first one or two. The same code worked with AVR, so do not understand why.

 

Ray.

0 件の賞賛
返信