SPI loop back with XDT512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI loop back with XDT512

1,847件の閲覧回数
MAC_HI
Contributor I
Hi iam working with XDT512 ,
 
SPI0 is master and SPI1 is slave
i want to loop back and send the data back to SPI0. 2BYTE data
Any application notes avaiable .please send to me immediately.
is there any internal loop back facility avaiable or i have to connect externally.???
 
Regards
MC
ラベル(1)
0 件の賞賛
返信
1 返信

1,179件の閲覧回数
Alban
Senior Contributor II
Hello,
 
There is no internal loopback between this 2 modules. You will have to put connections externally. No need to cross-over with SPI.
 
What does the Application Note you want would show ?
 
Alban.
0 件の賞賛
返信