S912ZVMC12F3 HAL/MCAL drivers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912ZVMC12F3 HAL/MCAL drivers

1,533 Views
tomrix
Contributor II

Hi,

I am currently starting a project with a S912ZVMC12F3 controller and I was wondering if there are Hardware Abstraction Layer (HAL) drivers / MCALs provided by NXP?

According to table at AUTOSAR® Software Architecture | NXP Semiconductors there are MCALS available, but not for S12Z MCUs. 
For S12ZVMC256 MagniV MCUs it is provided, so I was also wondering whether it can be used as the MCU is similar??

Appreciate support, cheers Thomas

 

0 Kudos
Reply
1 Reply

1,517 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @tomrix,

According to the release notes of the MCAL drivers, only the S12ZVMC256 is supported.

As you said, the MCUs are very similar - most of the modules like SPI, SCI, MSCAN are the same.

But there are differences too, refer to the RM, Table 1-3. S12ZVM Module Version Table.

Also, in general, the MCAL drivers requires more Flash and SRAM.

There is only 8kB of SRAM and 128kB of Flash on S12ZVMC12.

The MCAL comes with a Quality package that has Memory size reports for each driver.

 

Regards,

Daniel

 

0 Kudos
Reply