S912ZVMC12F1MKH

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S912ZVMC12F1MKH

4,918 次查看
七七曹
Contributor II

Communication is not connected  USB

clipboard11111111111111.png

微信图片_20180511172225.jpg

标记 (1)
5 回复数

4,646 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi 七七曹,

I'm not sure from your description if you follow the 3-phase Sensorless BLDC Development Kit|NXP, there you can find user guides and software. The software should be at first build and run in the CodeWarrior v10.7 and after that, you can open corresponding FreeMaster project. Do not forget set the Project -> Options.

I hope it helps you.

Best regards,

Diana 

4,645 次查看
七七曹
Contributor II

Hi Diana,

Thank you for your reply, The usb connect to my computer.

But my motor can not transient to sensorless mode. Only two phases have current and the other phase does not

User guides show me it like this :

0 项奖励
回复

4,645 次查看
pachamatej
NXP Employee
NXP Employee

Hello,

it seems to me that there is no current, only some noise. May I ask you to check the software you are using? Is it single-shunt or dual-shunt? Please refer to the Automotive Motor Control Development Solutions|NXP 

Your jumper settings indicate that you are using the dual-shunt. However, the software may be the single-shunt. If this is the case, you need to switch the jumpers J57 and J60.

Best regards,

Matej

0 项奖励
回复

4,645 次查看
七七曹
Contributor II

dual-shunt ;

jumpers J57 and J60 is connect 1-2;(Ia ib ic has it all)

i can not enter sensorless mode(position Mode)。Can you give me some advice??

0 项奖励
回复

4,645 次查看
pachamatej
NXP Employee
NXP Employee

Well, have you tried to download and install the latest SW? I just did and it works fine with the original devKit motor.

https://www.nxp.com/webapp/Download?colCode=MTRCKTSPNZVM128-SW&appType=license&Parent_nodeId=1428716... 

(MTRCKTSPNZVM128|Development Kit S12 MagniV|NXP )

Matej

0 项奖励
回复