S912ZVL64F0VLCR's BCTL PIN OUTPUT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S912ZVL64F0VLCR's BCTL PIN OUTPUT

跳至解决方案
4,459 次查看
Caleb1
Contributor I

What is the state of S912ZVL64F0VLCR's BCTL without program? What is the output voltage?

What is the status of the program? What is the output voltage?

0 项奖励
回复
1 解答
4,420 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Caleb1,

Out of the system reset, both regulators, the one with the internal ballast transistor and the one with the external ballast PNP are enabled.

danielmartynek_0-1692112469928.png

The external regulator has a slightly higher regulating point (5V) than the internal regulator (4.95V).

That means that the external regulator tries to regulate the VDDX voltage higher and opens the PNP (BCTL voltage is slightly lower than VSUP)

danielmartynek_1-1692112545889.png

 

Once the SW writes EXTXON = 0, INTXON = 1, the external regulator is disabled, that means Vemitter (VSUP) = Vbase (BCTL).

 

For this reason, the BCTL pin must be left unconnected if the PNP is not used.

 

Regards,

Daniel

在原帖中查看解决方案

0 项奖励
回复
7 回复数
4,185 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Caleb1,

While the debugger is attached, the MCU is in the Special mode, and the register can be written more than once.

But when the MCU runs stand-alone without the debugger, the MCU is in the Normal mode, and the register can be written only once.

Make sure that the register is written only once in the project.

S12ZVL RM rev.2.49, Section 4.3.2.1 Mode Register (MODE).

 

Regards,

Daniel

 

0 项奖励
回复
4,421 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Caleb1,

Out of the system reset, both regulators, the one with the internal ballast transistor and the one with the external ballast PNP are enabled.

danielmartynek_0-1692112469928.png

The external regulator has a slightly higher regulating point (5V) than the internal regulator (4.95V).

That means that the external regulator tries to regulate the VDDX voltage higher and opens the PNP (BCTL voltage is slightly lower than VSUP)

danielmartynek_1-1692112545889.png

 

Once the SW writes EXTXON = 0, INTXON = 1, the external regulator is disabled, that means Vemitter (VSUP) = Vbase (BCTL).

 

For this reason, the BCTL pin must be left unconnected if the PNP is not used.

 

Regards,

Daniel

0 项奖励
回复
4,195 次查看
Caleb1
Contributor I

Hi 

During the software debugging phase, setting registers makes it easy to open external pipes;

But after a slight increase, the external pipe couldn't be opened. Why is this?

What does the figure indicate as normal mode? When debugging, do you think it's not in normal mode?

What would it be like to write only once. Will the external pipes be turned off?

Thanks!

9.jpeg

 

0 项奖励
回复
4,216 次查看
Caleb1
Contributor I
 
0 项奖励
回复
4,442 次查看
ramprakash08
Contributor IV

The BCTL (Bootstrap Control) pin of the S912ZVL64F0VLCR is an output pin. Without a program, the state of the BCTL pin is typically undefined. It's important to note that the actual state can depend on the specific conditions of your system, such as power supply voltage, temperature, and the state of other pins.

The output voltage of the BCTL pin without a program can also vary depending on the conditions of your system. However, it's generally safe to assume that the output voltage will be within the range specified in the S912ZVL64F0VLCR's datasheet under the 'Electrical Characteristics' section.

When a program is running, the state and output voltage of the BCTL pin will depend on the specific instructions executed by the program. For example, if the program sets the BCTL pin to a high state, the output voltage will be close to the supply voltage (VDD). If the program sets the BCTL pin to a low state, the output voltage will be close to ground (VSS).

0 项奖励
回复
4,388 次查看
Caleb1
Contributor I

The current client's schematic design is the same as the schematic design provided

Adverse phenomenon: The normal output voltage of VDDX is 5V, but now it is 2.906V. The circuit behind this pin has been disconnected

Defective rate: The customer produced 60 sets and encountered 2 sets of this issue. If the power is cut off and then turned on again, the fault will disappear. I have done hundreds of power ups and downs, and this bad phenomenon will recur seven or eight times

The customer uses a normal board, erases the chip code, and then powers it on again. The output voltage of VDDX is 3.3V

0 项奖励
回复
4,378 次查看
danielmartynek
NXP TechSupport
NXP TechSupport
0 项奖励
回复