S12ZVMxEVB Board Schematics?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVMxEVB Board Schematics?

902 Views
ScottKerstein
Contributor III

Hello,

 

The MC9S12ZVM128MCBUG Users Guide states on the last page.  "For a complete list of schematics, see attachments with this document."  Are the attached schematics referring to the schematic blocks in various sections of the Users Guide, or is there a more complete schematics, or design files, available?

 

http://cache.nxp.com/files/microcontrollers/doc/user_guide/MC9S12ZVM128MCBUG.pdf?fpsp=1&WT_TYPE=User...

 

There is no schematic snip-it for the FAULT LED circuits.

 

Thanks, in advance

Scott

Labels (1)
0 Kudos
Reply
1 Reply

792 Views
RadekS
NXP Employee
NXP Employee

Hi Scott,

You are right, this sentence doesn’t make sense.

I will report that issue.

Please look at S12ZVMEVB page

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-magniv/s1...

In fact, this page and board user guide is shared for two boards - S12ZVML12EVB and S12ZVMC12EVB.

The difference is in assembled components.

The S12ZVML12EVB uses the S12ZVML128 integrating a LIN transceiver

The S12ZVMC12EVB uses the S12ZVMC128 integrating a voltage regulator controller for an external CAN transceiver

Please download appropriate schematic under “Downloads” tab.

Automotive motor control kits (include motor and example codes) are here:

http://www.nxp.com/products/software-and-tools/run-time-software/automotive-software-and-tools/motor...

For more documents and materials, please click there:

automotive-motor_control-download.png


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply