S12ZVMC256

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVMC256

2,349件の閲覧回数
18647340486
Contributor II

Dear all,

   

Initialization Mode Acknowledge — This flag indicates whether the MSCAN module is in initialization mode.
It is used as a handshake flag for the INITRQ initialization
mode request. Initialization mode is active when INITRQ = 1 and INITAK = 1. The registers CANCTL1,
CANBTR0, CANBTR1, CANIDAC, CANIDAR0–CANIDAR7, and CANIDMR0–CANIDMR7 can be written only by
the CPU when the MSCAN is in initialization mode.
0 Running — The MSCAN operates normally
1 Initialization mode active — The MSCAN has entered initialization mode


question:

1) INITAK——This flag indicates is not 0 after INITRQ=0.But all other register values are normal.

2)What causes MSCAN0 initialization to fail?

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,209件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi Katherine,

1. After exit initialization mode by writing INITRQ=0 we should wait for

INITAK = 0:  while (CAN0CTL1_INITAK){};

and Synchronized Status flag where SYNCH = 1 when MSCAN is synchronized to the CAN bus. 

2.  The MSCAN should not be active when initialization mode is entered.

More information can be found in the section "13.4.4.5 MSCAN Initialization Mode" in the RM rev.2.11

Also, I would like to recommend you the AN4975 Using MSCAN on the MagniV Family

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4975.pdf 

AN4975SW:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN4975SW.zip 

I hope it helps you.

Best Regards,

Diana

2,209件の閲覧回数
18647340486
Contributor II

Diana Batrlova,

   The above information is very helpful to me.

Thank you .

0 件の賞賛
返信