S12ZVL enable debugging in Full stop mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12ZVL enable debugging in Full stop mode

1,399件の閲覧回数
charu
Contributor I

Hi Team,

I have put the S12VL micro in Full stop mode using Stop instruction, after executing stop instruction loosing the debugger control.

Currently I am using PE debugger, let me know how to keep BDM mode active after execution of Stop instruction.

Thanks & Regards,

Charudatta

0 件の賞賛
返信
1 返信

1,386件の閲覧回数
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

 

After our discussion in a support ticket I would like to add some points here:

If you need to verify that you are in Full stop mode you can check the Bus clock. Since the Bus clock is stopped in Full-Stop mode, you can monitor the bus clock as ECLK provided ECLKCTL[NECLK] = 0.

In Full-Stop Mode the external oscillator and the oscillator clock monitor are disabled and unfortunately, I didn't find a way to debug the code by PE multilink interface in the Full-Stop Mode.

However, after MCU is awake from stop mode, you can go to Debug Configuration and select "Attach" as debug session type and click on "Debug".

Best regards,

Diana

 

 

Best regards,

Diana

0 件の賞賛
返信