S12ZVL LIN ldf file configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12ZVL LIN ldf file configuration

3,534 Views
b51447
NXP Employee
NXP Employee

Hi, 

Can we use .ldf GUI editor to configure the "Signal_encoding_types" and "Signal_representation" parts?

i can't find it in GUI editor sheet, however, there are some codes of  "Signal_encoding_types" and "Signal_representation" in the text editor sheet.

Thanks in advance.

Labels (1)
0 Kudos
Reply
3 Replies

3,073 Views
RadekS
NXP Employee
NXP Employee

Hi Remi,

The the "Signal_encoding_types" and "Signal_representation" provide additional information that does not change the behavior of the LIN cluster but provide hints for a presentation of the traffic by bus.

The GUI editor does not parse information in this section.

So users can’t use GUI editor to configure this section.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,073 Views
b51447
NXP Employee
NXP Employee

Hi, Radek,

Thanks for your answer. If customer want to add the information of these two parts. Could we add the information in the text editor window by ourselves? it is available?

0 Kudos
Reply

3,073 Views
RadekS
NXP Employee
NXP Employee

Hi Remi,

Yes, the information in these two parts may be / should be modified by a customer in the text editor.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply