S12Z TWR Board Availibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12Z TWR Board Availibility

1,567件の閲覧回数
marshallmontcha
Contributor I

I am so impressed by the Linear memory map of the s12z,  that I would like to buy a TWR system to build up with the TWR Geeks.

Is there any board out there?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,398件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Marshall,

I have here board X-TWR-S12ZVL32. However it is just prototype board (started with X).

Unfortunately I am afraid that this board will be probably not officially released and currently I do not know about any other TWR board for S12Z.

I already saw few prototype S12Z FRDM boards. I suppose that there is higher chance that these versions will be officially released. However I have to check it with application engineers.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,398件の閲覧回数
marshallmontcha
Contributor I

Thanks  Radek,

I notice a lot of TWR Geeks are using the Kinetis architecture and so I investigated the Kinetis MPU and I may have to change my favorite to include Bluetooth Low-Energy processor such as the K40_100.  Still interested in the S12z though.

Marshall

 Linear anomalies & Exception processing

0 件の賞賛
返信