S12Xe TIM and ECT Output Compare Pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12Xe TIM and ECT Output Compare Pins

1,325 Views
rayhall
Contributor V

When I look at the datasheet it has the external pin descriptions for TIM and ECT as the same pins ?

 

TIM

     22.2.8   IOC0 — Input Capture and Output Compare Channel 0 Pin

                  This pin serves as input capture or output compare for channel 0.

 

ECT

     14.2.8    IOC0 — Input Capture and Output Compare Channel 0

                   This pin serves as input capture or output compare for channel 0.

 

I see there that pin 4  has 5th function called TIMIOC0. Is the datasheet wrong and should be like this...

 

TIM

     22.2.8   TIMIOC0 — Input Capture and Output Compare Channel 0 Pin

                  This pin serves as input capture or output compare for channel 0.

 

ECT

     14.2.8    IOC0 — Input Capture and Output Compare Channel 0

                   This pin serves as input capture or output compare for channel 0.

 

Ray.

Labels (1)
0 Kudos
Reply
1 Reply

1,116 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

yes, it looks like typo. It would be better to use term TIMIOC however the chapter 22.2.8 says nothing about pin assignment it only describes pin function. The best approach is to look at Table 1-9. Pin-Out Summary to get pin-out.

Best regards,

Ladislav

0 Kudos
Reply