S12XDP512 PLL Circuit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12XDP512 PLL Circuit

2,100件の閲覧回数
sfb
Contributor I
Hi,
If I don't use PLL how should I connect the VDDPLL, VSSPLL, XFC pins. (Connect them to ground or 5V with resistor or nothing...)
ラベル(1)
0 件の賞賛
返信
1 返信

1,129件の閲覧回数
DPB
NXP Employee
NXP Employee
The VDDPLL, VSSPLL power domain is required for the oscillator input even if you are not using the PLL.
A decoupling capacitor (220 nF, X7R ceramic) should be placed between these supply lines, the internal voltage regulator supplies the power.

If PLL usage is not required, the XFC pin must be tied to VDDPLL.
0 件の賞賛
返信