S12 ZVML31 no GDU Flag

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12 ZVML31 no GDU Flag

3,281 Views
fabiansonnleitn
Contributor II

Hello,

 

I am using a S12 ZVML31 for a sensorless BLDC application. When the voltage drops down to 5.8V I do not get a GDUF error due to low voltage. Instead the signals on high side are switched with the low side for 400us.

 

Please find attache a scope screenshot.

purple - HD pin

blue - high side gate

yellow - low side gate

green - can be ignored

 

The voltage drop on HD is due to an active short on the lowside, for breaking.

 

Does anyone know this Problem?

 

all the best,

Fabian

Labels (1)
Tags (2)
3 Replies

3,103 Views
iggi
NXP Employee
NXP Employee

Hi,

The GDUF register will not indicate if HD voltage drops low. It indicates if HD voltage gets high by setting GHHDF bit.

How about to measure voltage on VLS_OUT pin too? And also, to check GLVLSF bit which indicates low level of VLS voltage supply.

Regards,

iggi

3,103 Views
fabiansonnleitn
Contributor II

Thank you!

did a update on

    GDUCTR_GHHDLVL and 
    GDUCTR_GVLSLVL

now it works flawless

0 Kudos
Reply

3,103 Views
iggi
NXP Employee
NXP Employee

Nice to hear that.

 If this post answers your question, please click the Correct Answer button.

Thank you!

0 Kudos
Reply