S12 XGATE Debugging

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S12 XGATE Debugging

2,148 Views
EmbeddedCoder
Contributor III
Hi all,
 
I am trying to choose a processor for my next project. My previouse project used a S12 device, and worked very well, the only problem I had towards the end was a bit of a squeeze on RAM resources. A good code trim seemed to sort it out!!
 
So I am thinking of going towards an S12XE device for my new project - they seem cheaper (I guess Freescale want to puch their new devices) and I am thinking that some of my driver code could be re-used, or at least retain the same style. As a bonus, I can also re-use the Metrowerks license I have!!
 
Debugging on the particular S12 device we chose previously was quite bad - the silicon had a bug that meant the trace facility in Metrowerks would not function, and only 2 breakpoints - felt like the 1980's...
 
So, my question is - is the debugging on the S12X devices any better?
Especially with the trace support - is this a useful feature - I'm thinking that with the additional XGATE accelaration there's a good chance the Trace module can get confused, or that debugging without Trace is a nightmare?
 
Any experiences, general gut feelings, recommendations gratefully received.
 
Thanks,
Mike
Labels (1)
0 Kudos
Reply
1 Reply

1,267 Views
DPB
NXP Employee
NXP Employee
Hello Mike

The on chip debug support for the S12X devices is enhanced with respect to the S12 devices.
The S12X DBG module offers 4 comparator channels with associated breakpoints that can be mapped to either CPU or XGATE and provide for breakpoints on PC addresses or data accesses.

Triggers for tracing use a state sequencer for more flexible control of trace begin or trace end.

Tracing of CPU and/or XGATE is supported by the DBG module. This does not confuse the DBG, but it can be slightly confusing trying to interpret the contents without a suitable debugging tool. For this reason it is recommended to use a debugger such as Codewarrior V4.6 or later. Codewarrior compiles a listing of the code flow from the trace buffer contents automatically.

The BDM and DBG modules are described in detail in chapters 7 & 8 of the S12XE- reference manual...
http://www.freescale.com/files/microcontrollers/doc/data_sheet/MC9S12XEP100RMV1.pdf?fpsp=1

DPB

0 Kudos
Reply