S12(X) family reprogrammable ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S12(X) family reprogrammable ?

2,834件の閲覧回数
daistar
Contributor I
1.is the S12(X) family reprogrammable and how may times??? 2.Is it possible to use other software instead of CW???? thats all for now..... tnx for replying...........

Alban Edit: PLEASE DO USE a meaninful subject !


Message Edited by Alban on 2007-05-25 01:18 PM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,672件の閲覧回数
daistar
Contributor I
and also where can i find the list of available instruction set for the S12(x) family,256 and 512???
0 件の賞賛
返信

1,672件の閲覧回数
DannyM83
Contributor III
Other compilers are available such as Cosmic.

The number of w/e cycles flash can handle can be found in the Electrical Characteristics Appendix in the Data book. Generally the values are minimum: 10K, typical 100k.

A complete instructrion set can be found in the Data book available on the relevent product page at freescale.com.

Hope that helps.

Danny
0 件の賞賛
返信