Reg. Erase / Write Cycles for EEPROM - MC9S12DJ64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reg. Erase / Write Cycles for EEPROM - MC9S12DJ64

2,843 Views
balajiprabhakar
Contributor I
Hi All,
 
In MC9S12DJ64 controller, How many ERASE/WRITE cycles are guaranteed for the EEPROM.
 
with regards,
 
Ganansekar.
Labels (1)
0 Kudos
Reply
2 Replies

1,596 Views
Lundin
Senior Contributor IV
The manual (A.32 NVM Reliability) says min 10000 cycles in temperatures below 0 dgr C, and min 100000 cycles in temperatures above 0 dgr C.
0 Kudos
Reply

1,596 Views
e_taylor
Contributor III
hello:
 
i don't know the value off hand but it should be listed under electrical spefications. the spec is for the entire temperature range and unless you are using the board in harsh temperatures the number is actually quite a low estimate.
 
 
regards,
 
ed
0 Kudos
Reply