Réponse slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Réponse slave

1,990 Views
karimaaissaoui
Contributor II

Bonjour,

Je me demande si le microcontrôleur HCS12P64 supporte l'émission des requêtes LIN maître et la réception des réponses esclave au même temps ou non, parce que j'arrive pas à récupérer les réponses slaves après avoir envoyé une requête LIN de DLC 0 

Labels (1)
2 Replies

1,900 Views
RadekS
NXP Employee
NXP Employee

Hi Karima,
Your original question is in the French language. Please be aware that we provide support only in the English language.
From google translator:
+++++++++++++++++++++++++
Hello,
I wonder if the HCS12P64 microcontroller supports sending LIN master requests and receiving slave responses at the same time or not, because I can not retrieve the slave responses after sending a DLC LIN request 0
+++++++++++++++++++++++++

I suppose that this your question was already answered in another thread:
https://community.nxp.com/message/855095

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,900 Views
karimaaissaoui
Contributor II

Hello Radek,

I hope you are well

You answered my question that I posted in the other group.

Thank you again Radek for your help.

You are the best.

Best regards.

2016-12-09 11:02 GMT+00:00 RadekS <[email protected]>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Réponse slave

reply from Radek Sestak

<https://community.nxp.com/people/RadekS?et=watches.email.thread> in *S12

/ MagniV Microcontrollers* - View the full discussion

<https://community.nxp.com/message/858953?commentID=858953&et=watches.email.thread#comment-858953>

0 Kudos
Reply