Problem connecting to HCS12X board using a Processor Expert project through serial monitor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem connecting to HCS12X board using a Processor Expert project through serial monitor

1,737 Views
Mounties
Contributor I

We are encountering errors when debugging.  We're only using the asynchronous bean, AS1-AnsynchroSerial.  The error generated is "CommError: 00000008 =  CE_FRAME; InQue: 5, OutQue: 0".  Any ideas as to what may be causing this or typical scenarios that generate this error?

Labels (1)
0 Kudos
Reply
1 Reply

1,352 Views
Mounties
Contributor I

We are pretty sure that the problem are based on the CPU settings and we're wondering if anyone knows the correct CPU settings for ProcessorExpert to work?

0 Kudos
Reply