PWM generation with using Quad Timer (56F8037)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PWM generation with using Quad Timer (56F8037)

2,005 Views
Dadis
Contributor I
Hi
I have a little problem. In my application with DSC 56F8037, Iam using all 6 PWM to drive 3ph DC/AC converter (for 6 IGBT), but I need to use another one PWM signal to drive input chopper circuit (in recuperation process). I read datasheet of 8037, there is a possibility use Quad-TImer in Fixed/Variable PWM mode.

My question : Can i use this for generate another PWM signal through any pin ? (for example GPIOD4 or GPIOD5). Will I have to trigger this pin in  Quad-timer interrupt?

Thanx a lot and sorry for my english.

David S.
Labels (1)
0 Kudos
Reply
1 Reply

1,071 Views
Dadis
Contributor I
So OFLAG pin you can put on external pin. But which pin is it ? Is this pin belong to Quad timer Ax/Bx (TA0-TA3 and TB0-TB3) ?
0 Kudos
Reply