OrCAD library for the S12ZVC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OrCAD library for the S12ZVC?

1,833 Views
fabriziom
Contributor I


HI,

 

i'm searching the OrCAD library for the S12ZVC, where can i download it?

Labels (1)
Tags (3)
2 Replies

1,628 Views
RadekS
NXP Employee
NXP Employee

Hi Fabrizio,

In attachment you could find OrCAD schematic and layout for VLG-MC9S12ZVC board.

I hope it helps you.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,628 Views
iggi
NXP Employee
NXP Employee

Hi,

that kind of file (if it exists at all) is not available for download on our website. I will check if we can get something similar from internal library and post it for download.

Regards,

iggi

0 Kudos
Reply