hello
When applying S912ZVML12AMKHR, using the pin9 BCTL of MCU plus PNP transistor to realize 12V to 5V, pin8 is configured as a high resistance input, I found that short-circuiting pin8 and pin9 leads to immediate damage to MCU, how to configure pin8 to avoid the problem of damage to MCU due to the short-circuiting of pin8 and pin9,
thanks!
How long will it take you to complete? "The current would need to be limited below 2.5mA (Table A-12, #17a).
AN4731 Understanding Injection Current on NXP Automotive Microcontrollers
https://www.nxp.com/docs/en/application-note/AN4731.pdf/ white screen "
Hello @yq1,
Absolute Maximum Ratings (RM, Table A-2) are 42V for BCTL and 6V for Digital I/O inputs.
"Absolute maximum ratings are stress ratings only. A functional operation outside these ranges is not guaranteed. Stress beyond these limits may affect the reliability or cause permanent damage of the device." (A.1.4).
When V_BCTL > V_PS5 and short-circuit, the injection currect can damage the MCU.
The current would need to be limited below 2.5mA (Table A-12, #17a).
AN4731 Understanding Injection Current on NXP Automotive Microcontrollers
https://www.nxp.com/docs/en/application-note/AN4731.pdf
Regards,
Daniel