MC9S12XS64: CW: 5.9.0: Selecting Bus frequency Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12XS64: CW: 5.9.0: Selecting Bus frequency Issue

2,875 Views
RaviKashi
Contributor I
Code:
void Config_CRG(void){   WORD counter = 0x0FFF;   /* RTIE=0 0 0 LOCKIE=0 0 0 SCMIE=1 0 */   CRGINT = 0x02; /* See above for selection */      /* Don't care as RTI not enalbed. */   RTICTL = 0x00;      /* WCOP=0 RSBCK=1 WRTMASK=1 0 0 CR2=1 CR1=0 CR0=0 */   COPCTL = 0x64; /* See above for selection COP times out in 2^20 clocks*/   POSTDIV      = 0x00; /* => fPLL = fVCO */       SYNR_VCOFRQ  = 0x01; /* 48MHz < fVCO<= 80MHz 01 */   REFDV_REFFRQ = 0x03; /* fREF >12MHz */   /**     * fVCO  = 2 × fOSC x (SYNDIV + 1) / (REFDIV + 1)    *    *     *           fVCO x ( REFDIV + 1 )    * SYNDIV = -----------------------  - 1    *                 2 × fOSC     *    * Let fOSC = 12MHz, fVCO = 48Mhz & REFDIV = 0x11     * Then, SYNDIV = 0x23    */      SYNR_SYNDIV  = 0x23;   REFDV_REFDIV = 0x11;       /* Wait for the PLL to Lock */#define SIMULATOR__#ifdef SIMULATOR__   while (counter--) #else   while ( ! CRGFLG_LOCK )  /* This will not happen with out hardware */#endif /* SIMULATOR */   {      PetWatchDogCOP();   }   /* CME=1 PLLON=1  FM1=0 FM0=1 FSTWKP=0 PRE=0 PCE=0 SCME=1 */   PLLCTL = 0xD1; /* See above for selection */      /* PLLSEL=1 PSTP=1 XCLKS=x 0 PLLWAI=0 0 RTIWAI=0 COPWAI=1 */   CLKSEL = 0xC1; /* See above for selection */}
 
I am trying this out on the Full Chip Simulation. *No hardware*
  • Planned Crystal: 12HMz
  • PLL Freq = VCO Freq (as POSTDIV = 0)
  • Desired PLL Freq : 48MHz => Desired BUS Freq = 24MHz

Problem: After the execution of the above code, the desired BUS freq jumps to 96MHz and after a few milliseconds of execution, gets an "Illegal_BP" reset. Can you please throw some light on where I may be going wrong?

Thanks, Ravi Shankar Kashi



Message Edited by Ravi Kashi on 2008-11-11 05:55 AM
Labels (1)
0 Kudos
Reply
2 Replies

1,466 Views
RaviKashi
Contributor I
Hello All,
 
   My bad!:robotmad: I had manually forced the Fosc in True-Time Simulator to 48MHz. As soon as I changed that back to 12MHz, everything worked as expected.
 
Thanks!
Ravi Shankar Kashi
0 Kudos
Reply

1,466 Views
chiusir
Contributor I
where do you get MC9S12XS?Can you help me ?
                                              roc  [email protected]


Message Edited by chiusir on 2008-12-29 12:29 PM
0 Kudos
Reply