MC9S12P Basic System

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S12P Basic System

1,825件の閲覧回数
Mishup
Contributor I

Hi, 

 

is anywhere something like a Recommended System Connections or Recommended PCB Layout ? It can be found in datasheets of many Freescale microcontrollers, but not for the S12P. Maybe is there other microcontroller with the same recommended connections? 

 

Any help would be appreciated! 

 

Thanks in advance.

 

Michael

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,635件の閲覧回数
CongTran
NXP Employee
NXP Employee

Don't know your HW board revision but let see attach for my board if it helps.

0 件の賞賛
返信

1,635件の閲覧回数
Lundin
Senior Contributor IV

I would advise against a 100nF decoupling cap on the reset line, I've encountered lots of problems with that in the past, for various S12 devices. The S12 apparently wants a pretty steep reset edge. 100pF or 47pF are probably better values. (And the BKGD line should have a similar cap.)

0 件の賞賛
返信