MC9S12NE64 with large (4MB) RAM buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S12NE64 with large (4MB) RAM buffer

3,272件の閲覧回数
okalex
Contributor I
Hello all,

I'm trying to decide on a microprocessor for a new design, and NE64 is very close to fulfilling all of our requirements, but not quite. The design requires Ethernet (I suppose on-chip Ethernet is not absolutely required, as we can add an external controller, but it would be very nice), I2C, and a 4MB external memory buffer. Looking at the datasheet for the NE64, it seems that the maximum size of memory that can be accessed is 1MB, if paging is used. Does anyone have experience adding more memory by using GPIO for additional address lines? Is this even possible?

Sincerely,
Alex Parkinson
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,889件の閲覧回数
Goz
Contributor I
Yup it is totally paossible I have used external memory with the NE64 in a product I designed, it is a pain in the backside as the memory lines are multiplexed, which means you need to use a de-multiplexer and a sample and hold device (D-type flip-flop based). Be aware, if you use external memory then you can ONLY use the ethernet interface at 10BaseT.
0 件の賞賛
返信

1,889件の閲覧回数
Nouchi
Senior Contributor II
Hi,

The MCF5223x family is the NE64 equivalent in the coldfire world, but the mcf5207 or mcf5208 will be better for your design , because it has a built-in SD/DDR RAM controller (up to 512Mbytes) and an integrated FEC you just have to add PHY device.
see:
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCF5207



Emmanuel
0 件の賞賛
返信

1,889件の閲覧回数
rocco
Senior Contributor II
Hi, Alex:

I can't say whether or not it is possible, but I can tell you that bit would be painful. Memory addressing is not a strong point for the S12s.

I would suggest looking at one of the Ethernet-enabled ColdFire processors, as they can access that much memory natively.
0 件の賞賛
返信