MC9S12C32 bit rate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S12C32 bit rate

1,212件の閲覧回数
wine
Contributor I

Hello,

 

I would like to ask about bit rate for MC9S12C32MFUE25. What happen if I change bit rate more than 20 or less than 20? It become slower  or faster for communication? I attach some file below...

 

Thanks in advance

ラベル(1)
0 件の賞賛
返信
1 返信

1,045件の閲覧回数
Lundin
Senior Contributor IV

I don't understand what you are asking for. If you increase the kilobits per second, I would indeed assume that more kilobits per second will be sent...

 

Though of course things aren't just that simple, what bit rate you can use depends on your clock prescaler settings. I believe that the CAN standard specifies a clock accuracy of 0.5%.

0 件の賞賛
返信