MC9S12C32 bit rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12C32 bit rate

1,191 Views
wine
Contributor I

Hello,

 

I would like to ask about bit rate for MC9S12C32MFUE25. What happen if I change bit rate more than 20 or less than 20? It become slower  or faster for communication? I attach some file below...

 

Thanks in advance

Labels (1)
0 Kudos
Reply
1 Reply

1,024 Views
Lundin
Senior Contributor IV

I don't understand what you are asking for. If you increase the kilobits per second, I would indeed assume that more kilobits per second will be sent...

 

Though of course things aren't just that simple, what bit rate you can use depends on your clock prescaler settings. I believe that the CAN standard specifies a clock accuracy of 0.5%.

0 Kudos
Reply