MC9S12 gpio injection current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S12 gpio injection current

1,638件の閲覧回数
angelo_d
Senior Contributor I

Dear all,

trying to figure out what is the injection current if i connect a 5V level to a 3.3VI/O powered mcu.

From datasheet seems it can reach > 3mA so over suggested limits, but not sure, since the diagram

is showing an example case for voltages > 5V.

 

Any help is appreciated.

regards

angelo

ラベル(1)
0 件の賞賛
返信
1 返信

1,427件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Angelo,

In fact, every S12 MCU GPIO pin is protected by ESD diodes against power supply rails.

So, any voltage higher than VDDX + voltage drop at ESD diode will generate injection current.

The same is valid for voltage smaller than VSSX - voltage drop at ESD diode.

Note: VDDA/VSSA for port AD.

The voltage drop at ESD diode for a fully opened diode is approximately 0.6 - 0.7V. However, we have to calculate rather with 0.3V where ESD diode starts open.

The maximum allowed continues injection current for one pin is 2.5mA.

However, the ESD diodes are not designed continuous conducting current and therefore we should avoid that situation if possible. It might have also side effects:

The ESD diode is heated by this injected current and influence neighborhood silicon.

The ADC results at neighborhood channels might be influenced.

The injection current might cause the fault (overvoltage) of the voltage regulator in MCU power save modes.

Please look at our application note AN4731 Understanding Injection Current on Freescale Automotive Microcontrollers for more details about injection current:

http://www.nxp.com/files/32bit/doc/app_note/AN4731.pdf

You might look also on slightly older application note AN2434 Input-Output Pin Drivers on HCS12 Family MCUs:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN2434.pdf

and AN2433 5V to 3V Design Considerations:

http://www.nxp.com/files/microcontrollers/doc/app_note/AN2433.pdf

Note: AN2433 is from 2002. There is plenty of newer voltage level translators which might be used:

http://www.nxp.com/products/discretes-and-logic/logic/voltage-level-translators

http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/ic-bus-portfo...

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信