License Problem with P&E USB Multilink Programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

License Problem with P&E USB Multilink Programmer

7,691 Views
MichaelA
Contributor I
Hey,
 
We have been using the SofTec HCS12X Starter Kit to develop our software, and now we have our own hardware, and need to program the HCS12X on our own Hardware with the P&E USB Multilink.  It works with programs under 1kB, but after 1kB, I get a license error thats as follows:
 
Feature 'HI407238: HC12 P&E ICD TArget' is running in demo mode!
To get an evaluation license, please send an email to [email protected]
maximum code size is 1024 bytes
 
Where can I check in CodeWarrior if everything is installed correctly.  We have the licenses to all of this, but always get this error.  Any suggestions on where to start concerning this error?  There a phone number I can maybe call to talk to someone about the license issue.
 
The SofTec board programs just fine with larger applications, but the error comes only when trying to program through the P&E.
 
Thanks,
 
Michael
Labels (1)
0 Kudos
Reply
4 Replies

3,355 Views
CrasyCat
Specialist III

Hello

Can you please do the following:

 - Start HI-WAVE and make sure you activate the Multilink connection
 - Select Help -> About
 - Can you please check teh content of the text box. What is written there?

Are you using a special edition, a standard edition, ...

CrasyCat

0 Kudos
Reply

3,355 Views
MichaelA
Contributor I
Have standard edition.  Pretty sure Multilink is enabled, because I can program the microcontroller just fine, as long as the program code is under 1 kB (but our larger program that needs to get loaded onto the hardware is well over 1kB).
 
Here's whats in the about box - license numbers blurred out for security (don't want to publish that on a forum...)
 

Directory: C:\Program Files\Metrowerks\CW for HCS12X V4.1\(CodeWarrior_Examples)\eigene Test\Finals\F_bootloader

Environment file: C:\Program Files\Metrowerks\CW for HCS12X V4.1\(CodeWarrior_Examples)\eigene Test\Finals\F_bootloader\P&E_ICD.ini

GENPATH=C:\Program Files\Metrowerks\CW for HCS12X V4.1\lib\hc12c\src;C:\Program Files\Metrowerks\CW for HCS12X V4.1\lib\hc12c\include;C:\Program Files\Metrowerks\CW for HCS12X V4.1\lib\hc12c\lib;C:\Program Files\Metrowerks\CW for HCS12X V4.1\lib\xgatec\src;C:\Program Files\Metrowerks\CW for HCS12X V4.1\lib\xgatec\include;C:\Program Files\Metrowerks\CW for HCS12X V4.1\lib\xgatec\lib

LIBPATH=C:\Program Files\Metrowerks\CW for HCS12X V4.1\lib\hc12c\include;C:\Program Files\Metrowerks\CW for HCS12X V4.1\lib\xgatec\include

OBJPATH=C:\Program Files\Metrowerks\CW for HCS12X V4.1\(CodeWarrior_Examples)\eigene Test\Finals\F_bootloader\bin

ABSPATH=C:\Program Files\Metrowerks\CW for HCS12X V4.1\(CodeWarrior_Examples)\eigene Test\Finals\F_bootloader\bin

TEXTPATH=C:\Program Files\Metrowerks\CW for HCS12X V4.1\(CodeWarrior_Examples)\eigene Test\Finals\F_bootloader\bin

Web: <http://www.metrowerks.com>

LM_LICENSE_FILE=

License File: C:\Program Files\Metrowerks\CW for HCS12X V4.1\license.dat

Application FLEXlm License Version: 2.000, 8.4a

Vendor daemon: metrowks

ETHERNET=**ETHERNET**

HOSTNAME=**COMPUTER**

DISK_SERIAL_NUM=**DISK_SERIAL**

FLEXID=**FLEXID**

HI404000 (metrowks, 2.000): HI-WAVE Engine (Single User License, FLEXID: **FLEXID**, registered)

HI491000 (metrowks, 2.000): Flash Programming Support (Single User License, FLEXID: **FLEXID**, registered)

0 Kudos
Reply

3,355 Views
CrasyCat
Specialist III

Hello

Please submit a service request through our on line support web site (http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=054670&tid=FSH).

Attach your license file and the whole content of the about box to the request.

CrasyCat

0 Kudos
Reply

3,355 Views
MichaelA
Contributor I
Hey,
 
I finally got a response from Mertrowerks - I had to add a line to my license.dat to enable programming with the P&E.  Works fine now.
 
- Michael
0 Kudos
Reply