LTC for MM9Z1J638

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LTC for MM9Z1J638

1,343 Views
qianlihu
Contributor I

Hi all

  I recently used KIT912J637EVME to measurement  of battery.  because consideration of power consumption,I use the LTC to wakeup from Low power mode(stop mode). for test, when wakeuped, delay 2 seconds and return to low power mode. And I find, the wakeup is working properly for several times(maybe several hundreds), and it could not return to low power mode again.

 

the LTC setting is followed:

 

159699_159699.pngpastedImage_2.png

 

Look forward to your favourable reply.

Thanks very much!

Labels (1)
0 Kudos
Reply
1 Reply

1,187 Views
iggi
NXP Employee
NXP Employee

Hi Qian,

From the subject and description, i am slightly confused if you are using MM9Z1J638 device or MM912J637. Which one? Or both...

Regarding the issue, you say it doesn't go to sleep mode.
Can you tell if the code runaways, or maybe gets stuck somewhere.

Do you do that test with BDM connected or not?

How about using other source of interrupts such as API or RTI?

Regards,

iggi

0 Kudos
Reply