Jenkin plugin for CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Jenkin plugin for CodeWarrior

3,753件の閲覧回数
pratibhasurabhi
Contributor V

Hi All,

I am using CodeWarrior for MCU "version : 10.7".


Q1 : Is there any jenkin plugin available for CodeWarrior such that i can use the same to build and update a CodeWarrior project ?

Q2 : How to use Jenkin plugin to update and build a CodeWarrior project?

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,603件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi, 

I have no personal experiences with Jenkins building, but you can probably start with installation of plugin.

1) Go to menu Help - > Install New Software. Add and select Juno repository into updater:

pastedImage_2.png

pastedImage_1.png

At the end of installation you need to restart CodeWarrior and new View is now available (menu Window-> Show View -> others -> Builds.

pastedImage_3.png

In this view you should be able to connect to Jenkins build server:

pastedImage_4.pngpastedImage_5.png

Unfortunatelly I don't have running Jenkins server installed so cannot test the connection.

Hope it helps.

Stan

0 件の賞賛
返信

3,603件の閲覧回数
pratibhasurabhi
Contributor V

Hi,

Thanks for the reply i was trying to install the suggested plugin from your suggested steps unfortunately it is showing error and plugin is not getting installed.

i am attaching the screenshot please have a look on it and suggest how to fix that.

pastedImage_1.png

0 件の賞賛
返信

3,603件の閲覧回数
pratibhasurabhi
Contributor V

Hi Stanislav,

Now i have successfully installed the plugin through the steps that you have mentioned above.

Still i am unable to connect jenkins with the plugin.

Can you please show me the steps by which jenkins build plugin can be integrated with jenkins.

0 件の賞賛
返信