Internal voltage regulator for s12Z controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Internal voltage regulator for s12Z controller

2,297件の閲覧回数
Pavani
Contributor I

Hello, 

I'm working on mc9s12zvl32mlf controller using code warrior software. I need to use internal voltage regulator of the controller for my application. I don't know which field should be modified so that CPMUVREGCTL register value changes to 0x01. By default in my code it is 0x02(external regulator). so, manually I am modifying the register value to 0x01(internal regulator) in processor expert generated code. so, can you please tell me the configuration in components to make CPMUVREGCTL register 0x01. Early reply is very much appreciated.

Thanks in advance.

 

0 件の賞賛
返信
2 返答(返信)

2,288件の閲覧回数
Pavani
Contributor I

Thank you very much @danielmartynek  

0 件の賞賛
返信

2,292件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Pavani,

I can't reproduce it.

The default configuration of the register is 0x01 (CW 11.1)

danielmartynek_0-1641296836450.png

But it can be changed anyway:

danielmartynek_2-1641297106801.png

 

Regards,

Daniel