IE Crash - NE64 demo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IE Crash - NE64 demo

3,592件の閲覧回数
NewBie1
Contributor I
I am a newbie. When I try to open the demo.htm for NE64 Open TCP, Internet Explorer crashes. I tried to install the VB 6 runtime files but even after that it is crashing. Please give me some ideas. I am using Windows NT Professional and IE 6.

Looking forward.
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,374件の閲覧回数
NewBie1
Contributor I
Someone please help me out. I want to access the variables in the memory page of the NE64 microcontroller. How do I do that using the demo software?
0 件の賞賛
返信

2,374件の閲覧回数
NewBie1
Contributor I
Thanks for the reply. It is working with WinXP now. I wanted to know how to make a webpage (similar to the demo) to access the variables in the memory page of the microcontroller.
0 件の賞賛
返信

2,374件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
Sounds like you should be reporting the crasher to Microsoft and not to this forum :smileywink:.
Anyway, instead of trying to manually fix IE, I would suggest to use an alternative browser instead.

Daniel
0 件の賞賛
返信

2,374件の閲覧回数
NewBie1
Contributor I
I am afraid, the activeX controls can only be used with IE I guess. For Firefox there are plugins available which only allow the proper functioning of some objects like Windows Media Player etc. Any other suggestions anyone?
0 件の賞賛
返信

2,374件の閲覧回数
J2MEJediMaster
Specialist I
Next logical step: borrow someone's system that has Windows XP installed on it to see if Win NT is missing a critical resource.

Also: how much RAM to you have in that box? Low memory conditions can cause all sorts of spurious problems.

---Tom

0 件の賞賛
返信