I need freeware for the HCS12E256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need freeware for the HCS12E256

2,970 Views
fiction
Contributor I
Hi Guys,
I am currently using the Code Warrior special edition for the HCS12E256.
With this special edition you are limited to only 32k of code space.
Is there any other freeware that i can use that does not limit me.

thanks guys
Labels (1)
0 Kudos
Reply
2 Replies

1,864 Views
JimDon
Senior Contributor III
Yes and No.
There is:
http://www.gnu.org/software/m68hc11/

However, you will have to pay for a debugger. NOICE will work with it and costs 99.00, one time charge.
Well worth the price.

Just wondering, have you actually written 32K of code ???
0 Kudos
Reply

1,864 Views
fiction
Contributor I
Hi Jim,
Yes my code is more 32k.
 
Thanks for the info
0 Kudos
Reply