I have a problem that s12zvm reset pin is low.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I have a problem that s12zvm reset pin is low.

1,345 Views
wonjaekim
Contributor I

I have a problem that s12zvm reset pin is low.

So. I can't download code.

I expect reset pin 5v but reset pin is low about 1v.

Why I have this problem??

I show you problem picture..

2 Replies

1,088 Views
RadekS
NXP Employee
NXP Employee

Hi Wonjae,

Just few notes:

The RESET pin is tied down during power up until reset sequence is finished (512~768 PLL cycles) or until the VDDX voltage reach LVR deassert value (approximately 3.13V).

 

The picture just told you that debugger cannot establish connection with the MCU. It may not have any relation to the RESET pin status itself. Please check voltage levels and reset pin levels.

If you use external debugger interface like Multilink Universal, please check also BDM connector orientation (on both sides),…

Best regards

Radek

1,088 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

There is a possibility that the MCU is reset repeatedly.

To verify, use an oscilloscope to measure voltage on the reset pin. 

Best regards,

Diana