I don't know 0~5KHz Freq for PWM function.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I don't know 0~5KHz Freq for PWM function.

ソリューションへジャンプ
2,309件の閲覧回数
Kr_Blue
Contributor I

.hi. Everyone.

 

I want know 0,1,2,3,4, ~  4998,4999,5000 Hz Freq for PWM function.

 

PWM Setting -> Channel clock period = 10KHz

                             input data = 0~1023

                             16bit PWM

 

ex)  if i want 1hz, 10KHz / 1Hz = 10K = PWMPER01 

                               10KHz / 2Hz = 5K = PWMPER01

                                                .

                                                .

                                                .

                                 10KHz / 700Hz = 3 = PWMPER01 

                                 10KHz / 701Hz = 3 = PWMPER01 

                                 10KHz / 702Hz = 3 = PWMPER01 

                                 10KHz / 703Hz = 3 = PWMPER01 

 

and I want 700,701,702,703Hz etc..... but  only PWMPER01 = 3 !!!!

so Output PWM is only 700Hz.

 

I want solution. 

input data is 1,2,3,4,5,6,7,8,etc.....

Output Hz is 1,2,3,4,5,6,7,8 etc Hz

ラベル(1)
0 件の賞賛
返信
1 解決策
1,806件の閲覧回数
kef
Specialist I

You need at least 25MHz PWM clock to be able to tune PWM frequency up to 5kHz with 1Hz resolution. 10kHz is certainly not enough.

Minimum PWM frequency in 16bits mode at 25MHz clock is 382Hz, so you you need to prescale 25MHz /2 for frequencies 191-381Hz, -"- 25MHz /4 for 95-190Hz, etc.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,807件の閲覧回数
kef
Specialist I

You need at least 25MHz PWM clock to be able to tune PWM frequency up to 5kHz with 1Hz resolution. 10kHz is certainly not enough.

Minimum PWM frequency in 16bits mode at 25MHz clock is 382Hz, so you you need to prescale 25MHz /2 for frequencies 191-381Hz, -"- 25MHz /4 for 95-190Hz, etc.

0 件の賞賛
返信
1,806件の閲覧回数
Kr_Blue
Contributor I

Thank you for you'r answer.

 

Your answer was the setting.

 

PWMPRCLK = 0x22; // BUS Clk / 4 = 3000000

                                      // BUS Clk = 12MHz

PWMSCLA=0x01;       // PWMPRCLK / (2*PWMSCLA) = 3000000 / (2 *1) = 1500000

PWMSCLB=0x01;

 

And good operation.

 

0 件の賞賛
返信