How to add external ram in Processor Expert cpu build options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add external ram in Processor Expert cpu build options

2,102 Views
AndersJ
Contributor IV
I want to add 256KB of external SRAM in normal expanded mode.
I am unable to add an external ram memory segment
using PE on the build options tab of the MC912SXD cpu bean.
* Name: RAM_External
* Qualifier: READ/WRITE
* Address: 140000 H
* Size 40000 H
 
At compile/link I get INTERNAL ERROR: at line 35 Unexpected status...... file: Drivers\HCS12\MC9S12_Linker.prg
 
Can anyone point out my error?
 
Thanks,
AJ
 
 
 
 
 
Labels (1)
0 Kudos
Reply
1 Reply

1,064 Views
ProcessorExpert
Senior Contributor III

This problem has been fixed in Processor Expert v2.99 for CodeWarrior v4.7. This version of Processor Expert is available as a service Pack on Freescale web.

best regards
Vojtech Filip
Processor Expert Support Team
UNIS
0 Kudos
Reply