How many channels of timer 0 and timer 1 are available as output compare in S12ZVL ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many channels of timer 0 and timer 1 are available as output compare in S12ZVL ?

2,155 Views
GoJuve
Contributor I

I've need of 15 PWM output in an application that use S12zvl 64 k microcontroller. 8 outputs are from PWM peripheral. Timer 1 is used for other purpose, so are not available. So I've need of 7 channels from Timer 0. In the Reference manual is written that Timer 0 has 6 channels, but in this link

S12ZVL Mixed-Signal MCU|MagniV|NXP

is written that Timer 0 has 8 channels (and Timer 1 4 channels). (reference manual is attached)

How many channels are available in Timer 0 and Timer 1 for S12ZVL 64,96,128K?

Thank you

Labels (1)
0 Kudos
Reply
1 Reply

1,827 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The reference manual is correct, S12ZVL64/94/128 MCUs have Timer_0 (6ch) and Timer_1(2ch).

The information on the web is not correct, it has been recently reported, it should be fixed.

 

Regards,

Daniel

0 Kudos
Reply