How can i Disable Interrupts from the debugger?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can i Disable Interrupts from the debugger?

2,659件の閲覧回数
pirate
Contributor I


Message Edited by pirate on 2008-06-05 09:08 PM
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,669件の閲覧回数
pirate
Contributor I
I am using MC9s12C64 and the Code warrior version is 5.7.0. I am want to disable interrupts once i stop at a breakpoint and step through code.

Thanks!!

0 件の賞賛
返信

1,669件の閲覧回数
allawtterb
Contributor IV


pirate wrote:
I am using MC9s12C64 and the Code warrior version is 5.7.0. I am want to disable interrupts once i stop at a breakpoint and step through code.

Thanks!!



If you are using the P&E Multilink or Cyclone Pro, in the hi-wave debugger it should be under:
MultilinkCyclonePro -> Communication -> Special Setup (tab) -> Disable Maskable ISR's when stepping

 
0 件の賞賛
返信