How can I use calibration page with CCP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I use calibration page with CCP

2,445件の閲覧回数
HSS6651
Contributor I

CCP example program of Vector support "SET_CAL_PAGE" commanf of CCP for C16X with DPP register.

void ccpSetCalPage( CCP_DWORD a )
{
  ccpCalPage = (CCP_BYTE)a;

    if (ccpCalPage==1) { /* RAM */
      #pragma asm
        mov DPP1,#11h
      #pragma endasm
    } else {             /* ROM */
      #pragma asm
        mov DPP1,#05h
      #pragma endasm
    }

}

 

But it's not support for HC12.

How can I make function like C16X with HC12 ot XGATE?

ラベル(1)
0 件の賞賛
返信
1 返信

1,736件の閲覧回数
VickLiui
Contributor I

forget CCP !

it's time for XCP

 

PAGE should be refer to EPAGE or RPAGE

0 件の賞賛
返信