How can I configure the download so that the internal eeprom is not erased?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I configure the download so that the internal eeprom is not erased?

602 Views
yankui666
Contributor III

When using CodeWarrior11 software to debug and download programs to the S12ZVM chip, the eeprom inside the S12ZVM chip will also be erased. How can I configure the download so that the internal eeprom is not erased?

采用CodeWarrior11软件给S12ZVM芯片调试下载程序的时候,S12ZVM芯片内部的eeprom也会一起擦除,怎么配置下载可以不擦除内部的eeprom

0 Kudos
Reply
1 Reply

467 Views
fqh
Contributor II

fqh_0-1732010369151.png

click Edit...

fqh_1-1732010419628.png

click Advanced Programming Options

fqh_2-1732010509712.png

check Preserve this Range (Memory Range 1)

 

0 Kudos
Reply